Arc Detection (PCIM 2014)
2014-06-04
The Arc Detection demo detects arc’s on the DC side of Solar inverters, using CT or a Rogowski coil front end sensor. The front end bandpass filter of 50kHz to 100kHz is developed using the AD8639 and sampled by the integrated ADC on the ADSP-CM403.
Arc Detection (PCIM 2014)
2014-06-04
The Arc Detection demo detects arc’s on the DC side of Solar inverters, using CT or a Rogowski coil front end sensor. The front end bandpass filter of 50kHz to 100kHz is developed using the AD8639 and sampled by the integrated ADC on the ADSP-CM403.
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}