Accelerometer FIFO Calculator
The Accelerometer FIFO Over-sampling Calculator is used to determine the necessary over-sampling ratio (OSR) to achieve an increased resolution. Select either the ADXL345 or ADXL346, and select whether you need to meet a system bandwidth requirement, or simply have a fixed accelerometer bandwidth you need to accomplish. Set the bandwidth, resolution, and max watermark inputs which meet your criteria, then hit the calculate button. The tool will determine how you should configure the accelerometer inorder to reach your input requirements, and calculate some output specifications using that configuration. For more detailed information about this tool please check out the complete document.