WLED

What is a WLED?

定义

WLED stands for white light emitting diode. WLED is a term usually associated with television and mobile phone LCD displays.

Although WLED is marketed as being in some way “different” or “superior” to standard LED, WLED, and LED technology are identical, using semiconductor materials. The white light produced is used as a ‘backlight’ for LCD displays and is created by applying an electric field to a blue (or UV) LED and then filtering the emitted light through a material of a different color (e.g., a yellow phosphor). The combination of the light and filter create a white (or almost white) light. In an LCD display, this light is then polarized using arrays of many liquid crystals, operating under the influence of variable electric fields, to create images on a screen.

What is the Difference Between WLED and OLED?

OLED (organic light emitting diode) technology uses organic (carbon-based) materials, instead of semiconductor (e.g., silicon or indium) materials used by standard LEDs. Each pixel of an OLED display comprises a red, green, and blue diode which emit light when a voltage is applied to them. Each diode can be switched on and off in different combinations and with different intensities to create images on a screen.

What are the Relative Advantages and Disadvantages of OLED/WLED?

The main advantage of OLED technology is that it allows displays to be much thinner (up to 10x) than displays made using LCD technology (with WLED backlight). Another important advantage is that because OLED displays do not need a backlight, they consume less power. This is critical for battery-powered displays (such as smartphones) as it means the battery does need to be charged as often. However, some disadvantages of OLED displays are that they are less water-resistant and the colors they produce deteriorates over time.

Find a term alphabetically: