概览

优势和特点

  • Full-featured evaluation board for the ADRF5062 
  • Easy connection to the test equipment
  • Thru line for calibration

产品详情

The ADRF5062 is a differential SPDT switch manufactured in the silicon on insulator (SOI) process.

This user guide describes the ADRF5062-EVALZ evaluation board, which was designed to evaluate the features and performance of the ADRF5062. Figure 1 on the user guide shows a photograph of the ADRF5062- EVALZ.

The ADRF5062-EVALZ uses the same evaluation board as ADRF5063-EVALZ.

Full specifications on the ADRF5062 are available in the ADRF5062 data sheet from Analog Devices, Inc. Consult the data sheet with this user guide when using the ADRF5062-EVALZ evaluation board.

相关产品