概览

产品详情

AD9119评估板连接ADI公司的数字模式发生器(DPG2),以便快速评估AD9119。 DPG2允许用户建立各种类型的数字矢量,并在任意AD9119工作模式下以该器件支持的速度传输至AD9119。 AD9119评估板通过USB以及随附的PC软件进行配置。

软件

ACE软件

ZIP
313 KB
ACE plug-in for Board.AD9129 1.2020.4400 [1月 23 20]
Plug-in for evaluating the AD9129 and AD9119 high-speed DACs.
EXE
157 MB
ACE Installer Software 1.30.3323.1470 [1月 10 25]
Analysis | Control | Evaluation (ACE) Software. Requires internet access. Run this executable to install ACE onto your computer. Required before installing the plug-in(s) above. Once ACE is installed, double-click on the plug-in package to install the plug-in.

硬件 (2)

控制器板