概览

产品详情

EVAL-AD7262EDZ是针对AD7262的全功能评估套件。此评估板可单独使用,也可与转换器评估与开发板EVAL-CED1Z配合使用。配合转换器评估与开发板使用时,用户可利用提供的软件对ADC进行详尽的性能分析。此软件还包括技术笔记,说明评估板在单独使用以及配合转换器评估与开发板使用时的操作与设置。

软件

评估软件

ZIP
330571 kB
AD7262 and AD7264 Evaluation Software
EVAL-AD7262EDZ and EVAL-AD7264EDZ software is available to the user in both Labview source code and in an executable version. The software download also includes source FPGA code used in the EVAL-AD7264EDZ system and an example C source file showing how to interface to the EVAL-AD7264EDZ evaluation system.

硬件 (1)

控制器板