REP025: 调谐在345MHz用于无线安全系统的LNA
Abstract
MAX2640的典型工作频率范围是400MHz至2500MHz。使用附加的匹配电路,它可以工作在345MHz,此时的增益约为17dB,噪声系数(NF)为1.4dB。用ADS对设计进行模拟,网络分析仪的观察结果证实了其工作性能。文中还给出了标准的S参数、电路原理图以及材料清单。
快速工程原型(rapid engineering prototypes)是Maxim应用工程师在实验室里建立并进行产品测试的实际电路。它们是新的射频工程设计的起点。
更多信息:
目标:调谐MAX2640使其工作在345MHz,用于无线安全系统的信号发射。
MAX2640的典型工作频率范围是400MHz到2500MHz,但是增加了Lnew和Cnew后可以使其工作在345MHz,此时拥有接近17dB的增益和1.4dB的噪声系数(NF)。将最初ZM1上边的输入导线切掉给电路板加入一个Lnew (大约43nH),Lnew和18pF的输入并联电容Cnew一起构成了LNA所需的输入匹配。匹配线ZM1也要移动一下。用模拟设计系统(ADS)进行仿真并通过网络分析仪得到新的匹配响应。
MAX2640是为蜂窝、PCS、GPS和2.4GHz ISM频段的应用设计的低成本超低噪声放大器。它使用+2.7V至+5.5V电源供电,消耗电流仅3.5mA并且具有低噪声系数、高增益和高三阶输入截取点(IP3)。MAX2640在900MHz典型的性能参数为:15.1dB的增益、-10dBm的输入IP3和0.9dB的噪声系数。
Schematic of MAX2640 Tuned for 345MHz Performance
Bill of Materials of Tuned MAX2640
S-Parameter Measurements Plot1,
S-Parameter Measurements Plot2
ADS Simulation Schematic
ADS Simulation Data