MAX3735A: 与DS1859接口时的特殊注意事项
Abstract
MAX3735A和DS1859广泛地用于155Mbps至2.7Gbps的SFP模块应用中。这两个器件配合使用时工作性能良好,可以高速运行、具有安全电路并可以实现SFP模块常用的监视功能。但是,在某些应用中,需要特别注意这两个器件的接口问题。
MAX3735A和DS1859广泛地用于155Mbps至2.7Gbps的SFP模块应用中。这两个器件配合使用时工作性能良好,可以高速运行、具有安全电路并可以实现SFP模块常用的监视功能。但是,在某些应用中,需要特别注意这两个器件的接口问题。