Design Note 267: High Efficiency White LED Driver Guarantees Matching LED Brightness

Introduction

White LEDs are widely used in small LCD backlight applications for simplicity, high reliability and low cost. However, due to variations in the forward voltage drop of white LEDs, matching the brightness becomes a major design consideration for multiple LED applications. Since LED brightness is proportional to current rather than voltage, a constant-current source driving LEDs in series should be used to ensure the same illumination of each LED. The LT1932 uses a constant-current step-up architecture that directly regulates the LED current and guarantees a constant light intensity in each LED, regardless of differences in their forward voltage drops. Its unique internal current source accurately regulates LED current even when the input voltage is higher than the LED voltage, greatly simplifying the battery/adapter power designs. The internal 36V switch is capable of driving up to eight LEDs in series with 20mA of LED current.

The LT1932 comes in the tiny 1mm, ThinSOT package. It operates at a constant 1.2MHz switching frequency, permitting the use of tiny, low profile chip inductors and capacitors to minimize circuit size and cost in space-conscious portable applications such as cellular telephones and handheld computers.

Li-Ion LED Driver for Four White LEDs

The white LED driver shown in Figure 1 is an ideal solution for Li-Ion powered, 4-LED backlight applications. The LT1932 and five external components require less than 0.65cm2 of printed circuit board space.

Li-Ion (or 5V) LED Driver for Four White LEDs

Figure 1a. Li-Ion (or 5V) LED Driver for Four White LEDs.

Li-Ion (or 5V) LED Driver for Four White LEDs

Figure 1b. Li-Ion (or 5V) LED Driver for Four White LEDs.

The constant-frequency step-up topology provides low noise, high efficiency and matched LED brightness along with adjustable current control. The LT1932 permits no LED current during shutdown, resulting in less than 1μA of battery current in the standby mode. The LED current is easily programmed over a range of 5mA to 40mA by selecting the value of RSET as shown in Table 1. By applying an additional DC voltage or a pulse-width modulated (PWM) signal to the RSET pin, the LED current can be adjusted for dimming or brightness control

Table 1. RSET Resistor Values
ILED (mA) RSET VALUE (Ω)
40 562
30 750
20 1.13k
15 1.50k
10 2.26k
5 4.53k

Dimming Control

The brightness of the LED can be easily adjusted using a PWM signal, a filtered PWM signal, a logic signal or a DC voltage. Five LED dimming schemes are shown in Figure 2. The LT1932 using PWM brightness control provides the widest dimming range and the purest white LED color over the entire dimming range. This results in better than a 20:1 dimming ratio without the undesirable blue tint common to white LED backlights. PWM controlled LED current is shown in Figure 3. Average LED current changes with duty cycle by switching between full current and zero current. This ensures that when the LEDs are on, they can be driven at the appropriate current to give the purest white light (at 15mA or 20mA) while the light intensity changes with the PWM duty cycle. See the LT1932 data sheet for more information about the dimming control methods shown in Figure 2.

Five Methods of LED Dimming

Figure 2. Five Methods of LED Dimming.

PWM Dimming Using the SHDN Pin

Figure 3. PWM Dimming Using the SHDN Pin.

Conclusion

For multiple white LED backlight applications, a constant current, series LED driver is required to ensure the light intensity matching in each LED. The constant current topology and 36V internal switch make the LT1932 an ideal solution for multiple white LED driver applications. The LT1932 features the purest white LED color dimming control, less than 1μA standby mode quiescent current, selectable current level, guaranteed LED brightness matching and extremely small circuit size making it well suited for portable cellular phone and handheld computer applications.

作者

David Kim

David Kim

Dave Kim is a Director for Automotive Systems Engineering for Power Products and Power electronics applications and systems design for more than 25yrs. He has joined Linear Technology (now part of Analog Devices) in 1997. Previously he has worked in various roles including product applications, field applications, technical sales / marketing and strategic applications manager.