DS2151, DS2152, DS2153, DS2154 Dallas Single Chip Transceiver Crystal Selection Guide
Abstract
Application Note 325 is a Crystal Selection Guide for these Dallas Single Chip Transceivers: DS2151, DS2152, DS2153, DS2154, DS21552, DS21554, DS21352, DS21354 and DS2155.
Specifications for selecting the appropriate crystal in a T1 or E1 application are given in the following order.
- Table 1: DS2155, DS21x5y, DS2154, and DS2152 Crystal Specifications
- Table 2: Recommended Crystal Manufacturers that meet DS2155, DS21x5y, DS2154, and DS2152 Crystal Specifications
- Table 3: Oscillator Manufacturers
- Table 4: DS2151 and DS2153 Crystal Specifications
- Table 5: Recommended Crystal Manufacturers that meet DS2151 and DS2153 Crystal Specifications
The DS2152, DS2154, DS21x5y, and DS2155 do not require a crystal for most applications. Typically, a clock derived from the system or supplied by an oscillator drives MCLK. If it is not a 1x clock, then appropriate divider can be used to drive the MCLK. For the DS2155, a 16.384MHz, 8.192MHz, 4.096MHz, 2.048MHz, or 1.544MHz clock must be applied at MCLK. ITU specification G.703 requires an accuracy of ±50ppm for both T1 and E1. TR62411 and ANSI specifications require an accuracy of ±32ppm for T1 interfaces. A prescaler divides the 16MHz, 8MHz, or 4MHz clock down to 2.048MHz. There is an on-board PLL for the jitter attenuator, which converts the 2.048MHz clock to a 1.544MHz rate for T1 applications. In an application that derives all timing from the network (loop timed), a crystal can be connected to MCLK and XTALD as shown in Figure 1. There is no pullability requirement for this crystal.
Figure 1. Crystal connection.
Specifications for selecting the appropriate crystal in a T1 or E1 application are given in Table 1. A list of crystal manufacturers is in Table 2. Table 5 lists oscillator manufacturers.
Parameter | Specification |
Parallel Resonant Frequency | 1.544MHz (T1), 2.048MHz (E1) |
Mode | Fundamental |
Load Capacitance | See Figure 1 |
Tolerance | ±50ppm |
Crystal Cut | AT |
Manufacturer | Address | Part |
Saronix | 141 Jefferson Drive Menlo Park CA 94025 650-470-7700 or 800-227-8974 |
Commercial Temp Range (T1, 3.088 MHz) NYP0308-XXGHE(L)* (E1, 4.096 MHz) NYP0409-XXGHE (L)* *Need to use divider for MCLK. |
Ecliptek | 3545 Cadillac Ave. Costa Mesa, CA 92626-1401 714-433-1200 |
Commercial Temp Range Crystal available for both T1 and E1 mode of operations. |
Manufacturer | Address | Part |
Saronix | 141 Jefferson Drive Menlo Park, CA 94025-1114 650-470-7700 or 800-227-8974 |
5V 8-Pin DIP SCS-DS-1046 1.544MHz SCS-DS-1047 2.048MHz |
3V 8-Pin DIP SCS-DS-1048 1.544MHz SCS-DS-1049 2.048MHz |
The DS2151 and DS2153 require a crystal that can be pulled off its center frequency. Table 5 lists manufacturers. The part numbers given are for leaded packages. Surface-mount devices typically do not meet the pullability specification. Some of the following manufacturers may offer surface-mountable packages in which the leads have been preformed (gull-winged) with a clip added to provide a third contact point.
Parameter | Specification |
Parallel Resonant Frequency | 6.176 (T1), 8.192 (E1) |
Mode | Fundamental |
Load Capacitance | 18pF to 20pF |
Tolerance | ±50ppm |
Pullability | CL = 10pF, ![]() CL = 45pF, ![]() |
Effective Series Resistance | 35Ω (max) |
Crystal Cut | AT |
Manufacturer | Address | Part |
M-Tron | 100 Douglas Ave. P.O. Box 630 Yankton, SD 57078-0630 605-665-9321 605-665-1709 |
Commercial Temp Range (T1, 6.176MHz) 4575-032 (E1, 8.192MHz) 4575-031 Industrial Temp Range (T1, 6.176MHz) 4144-002 (E1, 8.192MHz) 4144-001 Note: Do not use MP-1 Prefix |
Raltron | 2315 N.W. 107th Ave. Miami, FL 33172 305-593-6033 FAX: 305-594-3973 |
Commercial Temp Range (T1, 6.176MHz) A-6.176-18.5-DS (E1, 8.192MHz) A-8.192-18.5-DS Industrial Temp Range (T1, 6.176MHz) A-6.176-18.5-DSE (E1, 8.192MHz) A-8, 192-18.5-DSE |
Sunny-Emi Co. Suntrac (Dist) |
11925 Ventura Blvd. Studio City, CA 91604 818-509-8985 |
Industrial Temp Range (T1, 6.176MHz) SE 061-32 (E1, 8.192MHz) SE 081-30 |
JAN | 2341 Crystal Dr. P.O. Box 6017 Fort Myers, FL 33906-6017 941-936-2297 FAX: 941-936-3750 |
Commercial Temp Range (T1, 6.176MHz) JC6B18 (E1, 8.192MHz) JC8B18 |
Ecliptek | 3545 Cadillac Ave. Costa Mesa, CA 92626-1401 714-433-1200 |
Commercial Temp Range (T1, 6.176MHz) ECX-4173-6.176M (E1, 8.192MHz) ECX-3876-8.192M |
Saronix | Strategic Marketing, Inc. 624 W. University Suite 265 Denton, TX 76201 |
COMMERCIAL TEMP RANGE (T1, 6.176MHz) SRX5310(L) (E1, 8.192MHz) SRX5469(L) |
Maxim has qualified a sample of each device from the above manufacturers and has found that the device meets or exceeds our specifications. We do not conduct an ongoing qualification of these manufacturers.