Modular I/O Card for the IBM PC

RTI-820: Analog and Digital Inputs & Outputs for the PC, PC/XT, PC/AT; High Channel Capacity, Mixed I/O Types, Can Interface to 5B Signal Conditioners

The RTI-820, the newest member of the RTI-800 Series of PC Bus boards, is a modular input/output card that plugs into one of the long expansion slots in the IBM PC/XT/AT (or equivalent) personal computer. The board is compatible with a variety of interface panels to allow multiple, mixed I/O to be brought into and out of an IBM PC; it accommodates up to 64 multiplexed analog inputs, 16 multiplexed analog outputs, and 24 1-bit channels of digital I/O. Read full article



作者

Generic_Author_image

Brendon Howe