High-Performance, Low-Cost Bipolar-FET Op Amp

AD542K Has Vs=1mVmax, Tempco=10µV/°Cmax, Ib=25pAmax In Hermetic TO-99 Metal Can, Price is Only $3.50 (100's)

The AD542 is a monolithic FET-input operational amplifier in a TO-99 hermetically sealed metal can. The use of advanced bipolar-FET (bifet) technology, using ion-implantation, combined with laser-trimming at the wafer stage and user-oriented design, results in the highest performance available from amplifiers of this class. Read full article



作者

Generic_Author_image

Lew Counts

Generic_Author_image

Rich Frantz