Arduino Platform with Analog Devices Technology for Flexible Industrial Control

Abstract

Software-configurable systems enable industrial original equipment manufacturers (OEMs) to deliver unprecedented flexibility to the factory floor while simplifying product complexity. By introducing the Arduino OPTA platform for rapid development and deployment of automation systems, this article examines the features offered by Analog Devices technology integrated into the module, as well as complementary ADI solutions for complete signal chains in input/output (IO) modules.

Introduction

New software-configurable input/output (SWIO) features for control automation equipment allow any industrial IO function to be accessed from any pin, with the ability to configure channels anytime. This allows for customization at the time of installation—resulting in faster time to market, fewer design resources, and universal products that can be implemented broadly across various projects and customers.

To minimize the size of programmable logic controllers (PLCs) and enhance their configurability, Arduino has integrated the AD74412R into its micro PLC platform. The Arduino OPTA, shown in Figure 1, serves as an ideal platform for this quad-channel SWIO solution. It allows system architects and end users in building and process control environments to program it with ease using the Arduino PLC-integrated development environment(IDE). The SWIO single-chip solution combines functions for analog output, analog input, digital input, and resistance temperature detector (RTD) measurements, with serial port interface (SPI)-compatible data transfer and programming.

Figure 1. An OPTA module.
Figure 1. An OPTA module.

Arduino Module Detailed Information

Arduino designs, manufactures, and supports electronic devices and software, providing people globally with access to advanced technologies that interact with the physical world. Its products are straightforward, simple, and powerful, fulfilling the needs of users with ease. The PLC IO expansion exemplifies this, offering an easily configurable industrial instrument.

The module’s hardware supports full software configurability, enabling end users to program the input and output connections directly from the cloud. The flexibility provided by the AD74412R within the IO expansion connected to the OPTA PLC offers a fully configurable solution for Industry 4.0 applications. The interface is user friendly, allowing connections to various devices such as valves, 2-wire RTDs, pressure sensors, position sensors, 4-20 mA devices, buttons, switches, etc., all programmable via software. This component supports the implementation of Industry 4.0 in safe environments, with its robust design ensuring protection and IEC 61131-3 compliance. Additionally, the expansion includes two ports specifically for 3-wire RTD precision measurements.

The OPTA expansion enhances hardware capabilities while maintaining ease of programming through the Arduino IDE. The development tool offers a wide range of ready-to-use sketches, tutorials, and libraries, significantly reducing the time to market for the rail installer due to its low code approach and pre-mapped resources. Furthermore, the OPTA has the capability of real-time remote monitoring, firmware updates over-the-air through intuitive Arduino Cloud dashboards, and secure communication with a broad array of connected devices. Table 1 lists the technical specifications of the OPTA unit, with key features illustrated in Figure 2.

Table 1. OPTA Technical Specifications
Inputs 6× analog programmable
  • 4× 0 V to 10 V or 0/4-20 mA
  • 2× 0 V to 10 V or 0/4-20 mA or PT10’0
Outputs
  • 2× analog programmable: 0 V to 10 V or 0/4-20 mA
  • 4× PWM outputs
Analog Inputs Resolution 12-bit Analog Outputs Resolution 12-bit
Programming Languages from the Base Module From the main OPTA controller using
  • Arduino programming language via IDE
  • IEC 61131-3 via PLC IDE:
    • Ladder diagram (LD)
    • Function block diagram (FBD)
    • Sequential function chart (SFC)
    • Structured text (ST)
    • Instruction list (IL)
Expandability Through AUX port on the left and on the right. Available to connect to the OPTA base module or to expansions already connected. Enabling the connection of additional expansions in daisy chain.
Supply Voltage 24 V DC through dedicated pins Operating Temperature –20°C to +50°C (–4°F to +122°F)
IP Protection IP20 Certifications cULus listed, ENEC, CE
Figure 2. OPTA key features.
Figure 2. OPTA key features.

Complementary ADI Solutions

Complete universal IO modules can be achieved by integrating the AD74412R with the digital output capabilities of the MAX14906, along with solutions for power, protection, processing, security, and communication. The push toward Industry 4.0 and the digitization of factories necessitates higher IO counts, which are supported by integrated power solutions such as the ADP1032. This IC not only provides two regulated outputs but also offers galvanic isolation, safeguarding analog front ends by isolating SPI and GPIO signals and integrating an isolated DC-to-DC converter. Similarly, compact printed circuit board (PCB) designs are facilitated by using the MAX17671, which regulates the 24 V input to a module, minimizing the need for external components.

In addition to Linux drivers for the AD74412R, ADI provides no-OS drivers, enabling the development of SWIO solutions for low power microcontroller units (MCUs) such as the MAX32650. Recent security concerns have heightened legislative focus on cybersecurity in manufacturing systems, prompted by the EU Cyber Resilience Act, which mandates cybersecurity requirements for all “products with digital elements.” The MAX32650 features secure boot and key storage and can be paired with the MAXQ1065 cryptographic controller to provide a comprehensive root-of-trust and authentication solution.

Conclusion

SWIO using the AD74412R is ideal for remote IO modules, eliminating the need to deploy redundant fixed function IO channels in the space-constrained environment outside control cabinets. These modules are strategically placed within the control hierarchy to bridge traditional 4-20 mA IO to Ethernet-based communication. Edge-node Ethernet addressability facilitates the use of low level insights for cloud-based algorithms. T1L and advanced physical layer (APL) as implemented by the ADIN1110, a robust low power MAC-PHY, and the LTC9111 single-pair power over Ethernet (SPoE) power delivery (PD) controller offer an efficient, low overhead solution for this segment of the Ethernet ecosystem.

参考电路

Cyber Resilience Act–Factsheet.” European Commission, December 2023.

作者

Conal-Watterson

Conal Watterson博士

Conal Watterson博士是ADI公司接口与iCoupler®数字隔离器部的高级应用工程师,工作地点在爱尔兰利默里克。Conal拥有利默里克大学博士和工程硕士学位,自2010年以来发表了很多关于工业现场总线网络、诊断/可靠性、高速信号和隔离的论文和文章。他目前专注于集成隔离通信解决方案、高速接口和USB。

Alessandro Leonardi

Alessandro Leonardi

Alessandro Leonardi是ADI米兰分公司的现场应用工程师。他拥有米兰理工大学的电子工程学士和硕士学位。毕业后,他参加了ADI公司的现场应用培训生项目。

Giacomo Paterniani

Giacomo Paterniani

Giacomo Paterniani拥有博洛尼亚大学生物医学工程学位,并在摩德纳-雷焦·艾米里亚大学获得电子工程硕士学位。毕业后,他在摩德纳-雷焦·艾米里亚大学担任了一年研究员。2022年4月,他作为研究生现场应用工程师加入ADI公司的研究生项目。2023年4月,他成为一名现场应用工程师。