Accurate, Low-Cost, Easy-to-Use IC Multiplier

The AD534 Has Differential Inputs, Many Potential Applications; Laser-Trimmed on the Wafer to Accuracy Within 0.25% (AD534L)

The Analog Devices AD534 is a monolithic laser-trimmed multiplier having accuracy specifications conventionally associated with discrete modules. The AD534L guarantees an overall error of less than 0.25% of full scale, while the AD534J is within 1.0%. Read full article



作者

Barrie Gilbert

Barrie Gilbert

Barrie Gilbert是首位ADI院士,他“付出了毕生精力追求模拟技术的真谛。”他于1972年加入ADI公司,于1979年获封ADI院士,负责管理位于俄勒冈州比佛顿的西北实验室。Barrie于1937年出生于英国伯恩茅斯。在加入ADI公司之前,1954年,他在SRDE工作,研发第一代晶体管,之后加盟Mullard, Ltd.;后来还曾在Tektronix和Plessey研究实验室工作。Barrie是一名IEEE院士(1984年),一生获奖无数。他拥有约50项专利,发表过约40篇论文,与人合作出版多本著作,还是几家期刊的评审人。1997年,他获得了美国俄勒冈州立大学颁发的工程荣誉博士学位。