image
image
Analog Devices' commitment to ESG Analog Devices' commitment to ESG

The title of 2024 ESG Report - Resiliency and Responsibility - reflects two principles that have guided and enabled ADI's remarkable success for 60 years. They are core business principles and guideposts on the path to ADI's continued growth for decades to come.

Find the Report Here

Asia is a key market for Analog Devices, representing over 40% of the company's total revenue in fiscal year 2024. With a presence spanning over 50 years, ADI has established a strong foothold in these regions. ADI operates a network of facilities to support customer engagement in Asia and has a network of manufacturing sites across these regions, including Chonburi, Thailand, Penang, Malaysia and Cavite, Philippines. To better support customers through cutting-edge technologies and solutions, ADI has 8 design centers across Asia. ADI's strong regional presence is further supported by an extensive network of authorized sales and distribution channels across these regions.

Featured Technology

Integrated SoC shrinks the size of the 4-20 mA smart transmitter

The 4-20 mA current loop offers a common technique for transmitting sensor information such as temperature and pressure in industrial process-monitoring applications.

Download Now

High fidelity PCB design for multichannel beamformers

Part 1 discusses designing PCBs with highly accurate 50 Ω trans-mission lines.Part 2 will discuss isolation between transmission lines,how isolation affects beamformer IC performance.

Download Now

How to convert voltages using a high voltage buck controller without a transformer

Switch-mode power supplies without transformers are typically used at lower voltage levels. new devices such as high voltage buck controllers can be used instead.

Download Now

ADI In Social Media

Contact Us

Analog Devices International, LLC Singapore Branch

Address: Solaris@Kallang 164
164 Kallang Way
#07-09 Singapore 349248
Phone: +65 6427 8430

Analog Devices India Private Limited

Address: Salarpuria Nova
No. 1, Varthur Road
Nagavarpalya, Bengaluru 560093
Email: cic.asia@analog.com


welcome-in-feedback   welcome-in-ezchina-1