Search

You searched for “EVAL-AD4854”
Filters
Filters
Site Section
- 5
Results on Analog.com
Relevance
Sort by
- Evaluation Board & KitThis evaluation board for the ADG854 is fitted with three audio connectors that allow the user to switch between two audio sources or to switch an audio source between two speakers. The ADG854 offers ultralow on resistance of less than 1 Ω over the full temperature range and all signals applied to the switch can be monitored using the test points provided.
- Evaluation Board & KitThe EVAL-AD4857FMCZ is designed to demonstrate the performance of the AD4857 and to provide access to many included configuration options that are accessed via a simple ACE plug-in graphical user interface (GUI). The AD4857 is a fully buffered, 8-channel simultaneous sampling, 16-bit, 1 MSPS data acquisition system (DAS) with differential, wide common-mode range inputs. The EVAL-AD4857FMCZ on-board components include the following: The LTC6655 high precision, low drift, 4 …
- Evaluation Board & KitPlease be aware that this product is not compatible with current Microsoft operating systems. In addition, the interface cable between computer and the evaluation board requires a parallel printer cable not available on newer computers. For new designs, the AD9956 and AD9912 should be considered.
- AD4857Recommended for new designsProductSimultaneous Sampling A/D ConvertersBuffered, 8-Channel Simultaneous Sampling, 16-Bit 1 MSPS DAS
- AD4858Recommended for new designsProductSimultaneous Sampling A/D ConvertersBuffered, 8-Channel Simultaneous Sampling, 20-Bit 1 MSPS DAS
- AD4855Recommended for new designsProductSimultaneous Sampling A/D ConvertersBuffered, 8-Channel Simultaneous Sampling, 16-Bit 250 kSPS DAS
- ADG854ProductionProductSingle-Supply Analog Switches and Multiplexers0.5 Ω CMOS 1.8 V TO 5.5 V Dual SPDT/2:1 MUX Mini LFCSP Package
- User GuideThe EVAL-AD4857FMCZ is designed to demonstrate the performance of the AD4857 and to provide access to many included configuration options that are accessed via a simple ACE plug-in graphical user interface (GUI).
- User GuideThis user guide describes the EVAL-ADG854EBZ evaluation board for the ADG854, which is a low voltage CMOS device that contains two independently selectable, single-pole, doublethrow (SPDT) switches.
- <<
- <
- 1
- >
- >>