Low Dropout Regulators—Why the Choice of Bypass Capacitor Matters

Widely seen as a panacea for solving noise-related issues, capacitors deserve more respect. Designers often think that adding a few capacitors will solve most noise problems, but give little thought to parameters other than capacitance and voltage rating. Like all electronic components, however, capacitors are not perfect. Instead, they possess parasitic effective series resistance (ESR) and inductance (ESL); their capacitance varies with temperature and voltage; they are sensitive to mechanical effects.

Designers must consider these factors when selecting bypass capacitors—as well as for use in filters, integrators, timing circuits, and other applications where the actual capacitance value is important. An inappropriate choice can lead to circuit instability, excessive noise and power dissipation, shortened product life, and unpredictable circuit behavior.

Capacitor Technologies

Capacitors are available in a wide variety of form factors, voltage ratings, and other properties to meet the requirements of diverse applications. Commonly used dielectric materials include oil, paper, glass, air, mica, polymer films, and metal oxides. Each dielectric has specific properties that affect its suitability for a particular application.

In voltage regulators, three major classes of capacitors are commonly used as voltage input- and output bypass capacitors: multilayer ceramic, solid-tantalum electrolytic, and aluminum electrolytic. The Appendix provides a comparison.

Multilayer Ceramic

Multilayer ceramic capacitors (MLCC) combine small size, low ESR, low ESL, and wide operating temperature range, making them the first choice for bypass capacitors. They are not without faults, however. Depending on the dielectric material, the capacitance can vary dramatically with temperature, dc bias, and ac signal level. In addition, the piezoelectric nature of the dielectric material can transform vibration or mechanical shock into an ac noise voltage. In most cases, this noise tends to be on the order of microvolts, but in extreme cases, mechanical forces can generate noise in the millivolt range.

Voltage-controlled oscillators (VCOs), phase-locked loops (PLLs), RF power amplifiers (PAs), and other analog circuits are sensitive to noise on their power-supply rails. This noise manifests itself as phase noise in VCOs and PLLs, amplitude modulation in RF PAs, and display artifacts in ultrasound, CT scans, and other applications that process low-level analog signals. Despite these imperfections, virtually every electronic device uses ceramic capacitors due to their small footprint and low cost. For regulators used in noise-sensitive applications, however, designers must carefully evaluate their side effects.

Solid Tantalum Electrolytic

Solid tantalum capacitors are less sensitive to the effects of temperature, bias, and vibration than ceramic capacitors. A recent variation uses a conductive polymer electrolyte instead of the usual manganese dioxide electrolyte, providing improved surge-current capability and eliminating the need for a current-limiting resistor. Lower ESR is an additional benefit of this technology. Solid tantalum capacitors have a stable capacitance with temperature and bias voltage, so the selection criteria need only account for the tolerance, voltage derating at the operating temperature, and maximum ESR.

Conductive polymer tantalum capacitors with low ESR cost more and are somewhat larger than ceramic capacitors, but may be the only choice for applications that cannot tolerate noise due to piezoelectric effects. The leakage current of tantalum capacitors is much larger than for equal-value ceramic capacitors, however, rendering them unsuitable for some low-current applications.

A drawback of the solid polymer electrolyte technology is that this type of tantalum capacitor is more sensitive to the high temperatures encountered in the lead (Pb)-free soldering process, with manufacturers typically specifying that the capacitors not be exposed to more than three soldering cycles. Ignoring this requirement in the assembly process can cause long-term reliability issues.

Aluminum Electrolytic

Conventional aluminum electrolytic capacitors tend to be large and have high ESR and ESL, relatively high leakage current, and limited service lifetimes—measured in thousands of hours. OS-CON capacitors employ an organic semiconductor electrolyte and an aluminum foil cathode to achieve low ESR. Although related to solid polymer tantalum capacitors, they actually preceded tantalum capacitors by 10 years or more. With no liquid electrolyte to dry out, the service lifetime of OS-CON type capacitors is better than that of conventional aluminum electrolytic capacitors. Most are limited to 105°C, but OS-CON type capacitors capable of 125°C operation are now available.

Although the performance of the OS-CON type capacitor is better than that of conventional aluminum electrolytic capacitors, they tend to be larger and have higher ESR than ceramic or solid polymer tantalum capacitors. Like solid polymer tantalum capacitors, they do not suffer from the piezoelectric effect, so they are suitable for use in low-noise applications.

Selecting Capacitors for LDO Circuits

Output Capacitor

Low-dropout regulators (LDOs) from Analog Devices can operate with small, space-saving ceramic capacitors as long as they have low effective series resistance (ESR); the ESR of the output capacitor affects the stability of the LDO control loop. A minimum capacitance of 1 µF with a maximum ESR of 1 Ω is recommended to ensure stability.

The output capacitance also affects the regulator's response to changes in load current. The control loop has finite large-signal bandwidth, so the output capacitor must supply most of the load current for very fast transients. When the load current switches from 1 mA to 200 mA at 500 mA/µs, a 1-µF capacitor, unable to supply enough current, produces a load transient of about 80 mV, as shown in Figure 1. Increasing the capacitance to 10 µF reduces the load transient to about 70 mV, as shown in Figure 2. Increasing the output capacitance further, to 20 µF, allows the regulator control loop to track, actively reducing the load transient as shown in Figure 3. These examples use the ADP151 linear regulator with a 5-V input and a 3.3-V output.

Figure 1
Figure 1. Transient response with COUT = 1 µF.
Figure 2
Figure 2. Transient response with COUT = 10 µF.
Figure 3
Figure 3. Transient response with COUT = 20 µF.

Input Bypass Capacitor

Connecting a 1 µF capacitor from VIN to GND reduces the circuit's sensitivity to printed circuit board (PCB) layout, especially when long input traces or high source impedance are encountered. Increase the input capacitance to match the output capacitance when more than 1 µF is required on the output.

Input and Output Capacitor Properties

The input and output capacitors must meet the minimum capacitance requirement at the intended operating temperature and working voltage. Ceramic capacitors are available with a variety of dielectrics, each with different behavior vs. temperature and voltage. X5R or X7R dielectrics with a 6.3-V to 10-V voltage rating are recommended for 5-V applications. Y5V and Z5U dielectrics have poor characteristics vs. temperature and dc bias, so they are not suitable for use with LDOs.

Figure 4 shows the capacitance vs. bias voltage characteristic of a 1-µF, 10-V X5R capacitor in a 0402 package. The capacitor's package size and voltage rating strongly influence its voltage stability. In general, a larger package or higher voltage rating will provide better voltage stability. The temperature variation of the X5R dielectric is ±15% over the –40°C to +85°C temperature range and is not a function of package or voltage rating.

Figure 4
Figure 4. Capacitance vs. voltage characteristic.

To determine the worst-case capacitance over temperature, component tolerance, and voltage, scale the nominal capacitance by the temperature variation and tolerance, as shown in Equation 1:

 CEFF = CBIAS × (1 – TVAR) × (1 –TOL)
   (1)

Where CBIAS is the nominal capacitance at the operating voltage; TVAR is the worst-case capacitance variation over temperature (as a fraction of 1); TOL is the worst-case component tolerance (as a fraction of 1).

In this example, TVAR is 15% from –40°C to +85°C for an X5R dielectric; TOL is 10%; CBIAS is 0.94 µF at 1.8 V, as shown in Figure 4. Using these values in Equation 1 yields:

CEFF = 0.94 µF × (1 – 0.15) × (1 – 0.1) = 0.719 µF 

The ADP151 specifies a minimum output bypass capacitance of 0.70 µF over the operating voltage and temperature range, so this capacitor meets this requirement.

Conclusion

To guarantee the performance of an LDO, the effects of dc bias, temperature variation, and tolerance of the bypass capacitor must be understood and evaluated. In applications that require low noise, low drift, or high signal integrity, the capacitor technology must also be considered. All capacitors suffer from the effects of nonideal behavior, so the capacitor technology chosen must match the needs of the application.

Appendix

Figure A
Figure A. Capacitors commonly used for bypassing power supply rails.

Clockwise from top, scale in millimeters:
100-µF/6.3-V polymer solid aluminum capacitor
1-µF/35-V and 10-µF/25-V solid tantalum capacitor
1-µF/25-V, 4.7-µF/16-V, 10-µF/25-V multilayer ceramic capacitor
10-µF/16-V, 22-µF/25-V aluminum electrolytic capacitor

Comparison of Critical Parameters of Various Capacitor Technologies

Capacitor Technology Effective Series Resistance Effective Series Inductance Voltage Stability Temperature Stability Sensitivity to Vibration Capacitance / Unit Volume
Aluminum Electrolytic Highest Highest Good
Lowest
Low
Low
Solid Tantalum Medium Medium Best Good Low
High
Polymer Solid Aluminum Low Low Best
Good
Low
High
Multilayer Ceramic Lowest Lowest
Poor Good
High Medium

References

AN-1099 Application Note, Capacitor Selection Guidelines for Analog Devices, Inc., LDOs

Author

Glen-Morita

Glenn Morita

Glenn Morita graduated from Washington State University with a B.S.E.E. in 1976. His first job out of school was at Texas Instruments, where he worked on the infrared spectrometer instrument for the Voyager space probe. Since then, Glenn has worked as a designer in the instrumentation, military and aerospace, and medical industries. In 2007, he joined ADI as an applications engineer with the Power Management Products Team in Bellevue, WA. He has over 25 years of linear and switch-mode power supply design experience at power levels ranging from microwatts to kilowatts. Glenn holds two patents for harvesting energy from body heat to power implantable cardio-defibrillators and an additional patent for extending battery life in external cardio-defibrillators. In his spare time, he enjoys collecting minerals, faceting gemstones, photography, and visiting national parks.