Search

Filters
Filters
Tools and Models
- 1
Site Section
- 34
Results on Analog.com
Relevance
Sort by
- Evaluation Board & KitThis evaluation board provides full access to all analog and digital I/Os on the ADAU1772. The ADAU1772 core is controlled by Analog Devices, Inc., SigmaStudio™ software, which interfaces to the board via a USB connection. This evaluation board can be powered by a single AAA battery, by the USB bus, or by a single 3.8 V to 6 V supply; any of these are regulated to the voltages required on the board …
- Technical ArticlesMar 20, 2025… a high performance passive crossover (Figure 3) and powered with a Behringer NX1000 amplifier, which can output 300 W per channel at 4 Ω with a THD of 0.05%. For DSP system measurements, the Analog Devices EVAL-ADAU1467Z was used with SigmaStudio, a free programming environment for SigmaDSP® products. SigmaStudio is a block-based IDE graphical user interface that includes such features as EQ, crossovers, routing, delays, metering, and limiting. The output of …
- User GuideThis user guide details the design, setup, and operation of the EVAL-ADAU1466Z evaluation board.
- Frequently Asked QuestionThe EVAL-ADAU1401EBZ includes flexible connections to all I/O and control features of the IC. The PCBs for these are 6"x6". The EVAL-ADAU1701MINIBZ is a 2"x2.5" PCB that includes stereo line-level I/O, along with a 2W stereo Class-D output using an SSM2306. Both evaluation kits include a full version of SigmaStudio and a USBi interface board. For most evaluation needs, the mini board is the best choice …
- User GuideThe EVAL-ADAU1861EBZ provides all the analog and digital inputs and outputs on the ADAU1861.
- User GuideThis user guide explains the design and setup of the EVAL-ADAU1787Z evaluation board.
- User GuideThis user guide explains the setup of the EVAL-ADAU1797Z evaluation board.
- User GuideThis evaluation board provides full access to all analog and digital inputs/outputs on the ADAU1777.
- User GuideThe EVAL-MICCANVASZ microphone canvas provides a platform for the development and evaluation of microphone beamforming arrays.