AD6480
ObsoleteAn AFE Chip, Part of the EAGLE ADSL CPE Chipset
Viewing:
Part Details
As part of the EAGLE ADSL CPE chipset, the AD6480 is an analog front end (AFE) chip with an integrated line driver, receiver, and filtering circuitry. When paired with one of the following ADSL data pumps, it provides complete ADSL modem chipsets as follows:
The AD6480 MUST be ordered with one of the datapumps listed above and is not offered as a stand-alone part.
Latest Discussions
No discussions on AD6480 yet. Have something to say?
Start a Discussion on EngineerZone®