Search

You searched for “de”
Filters
Filters
Tools and Models
- 1,736
- 362
- 346
- 5
Site Section
- 59,521
- 1,982
- 108
- 94
- 90
- 36
Results on Analog.com
Relevance
Sort by
- Design NoteReference design for an automotive antenna features an AM/FM low-noise amplifier (LNA) for active antenna modules. Article details the capabilities, features, and ease of design with an AM/FM active antenna LNA.
- Design NoteDescribe the key system parameters that should be considered when designing a low cost, low component count unassisted commercial GPS receiver.
- Design NoteThis article illustrates an output-matching network and component values for the MAX1472, a crystal-referenced, phase-locked loop (PLL) transmitter that transmits OOK/ASK data in the 300MHz to 450MHz frequency range.
- Technical ArticlesSep 27, 2002Optimize the RF input and output matching circuits on the MAX2648 LNA. A small stub insures stability.
- Design NoteHow to use the DS26504 Jitter Attenuator to avoid phase slip and wander.
- Design NoteThe backlight for a handheld computer’s liquid crystal display should be efficient, compact and inexpensive. The two primary competing backlight solutions, white LEDs and Cold Cathode Floresent Lamps (CCFLs), satisfy some of these requirements but neither excel in all.
- Technical ArticlesSep 18, 2012Determine the half-IF spurious requirement for a high-performance base-station receiver and select the appropriate mixer with an understanding of how the mixer's IP2 and second-order response performance relates to the half-IF spurious requirement.
- Technical ArticlesApr 10, 2009The following application note describes Maxim's approach of how to incorporate the powerful features of the MAX6974 to realized an LED-based video display board.
- Technical ArticlesDec 23, 2005This application note will present the cause of the internal ESD diode failure for MAX2140. It will provide the design guides and the example of the case calculations.
- Design NoteThis application note discusses a design for a phantom antenna power-supply system compatible with the Digital Satellite Equipment Control (DiSEqC) communication standard.