Search

You searched for “ADSP-MSP58”
Filters
Filters
Site Section
- 53
Results on Analog.com
Relevance
Sort by
- Analog DialogueThis article discusses in detail the main microcontroller’s software, which is responsible for guaranteeing the smooth functioning of processes.
- Design NoteIn dual feed applications, supply connections can be erroneously wired, causing damage to the load. An ideal diode solution using the LTC4355 and LTC4354 provides protection similar to Schottkys, but with much lower power dissipation.
- Technical ArticlesDec 1, 2001High output fans that work full time do not last very long (their bearings wear out), are not very efficient (they use power also), and are noisy (especially when their bearings wear out).
- Analog DialogueTraditional bipolar PS usually equipped with three output terminals: positive, negative and GND. In contrast, two-quadrant PS carries two output terminals, one is GND and another can be positive or negative. The output voltage can be regulated relative to the GND by the control signal. in a full range from the minimum negative to the maximum positive.
- GlossaryAn H-bridge is a circuit diagram which resembles the letter "H." The load is the horizontal line, connected between two pairs of intersecting lines. It is very common in DC motor-drive applications where switches are used in the "vertical" branches of the "H" to control the direction of current flow, and thus the rotational direction of the motor.
- Technical ArticlesJun 10, 2016The no-opto isolated flyback parts from Linear need no opto-coupler or LT1431 shunt regulator for regulation. They sense the isolated output voltage directly from the primary-side waveform. This simplifies the design, allows for a smaller solution size and only requires one component crossing the isolation barrier. The load, line and temp drift is less than ±5%. Several off-the-shelf transformers are shown in the data sheets making it easy to complete …
- Product Selector Card
PDF
587.00K
- Application Note
PDF
633.00K