AD1881
ObsoleteAC ’97 SoundMAX® Codec
Part Details
The AD1881 is the first audio Codec to meet the Audio Codec ’97 2.0 and 2.1 Extensions. In addition, the AD1881 SoundMAX® Codec is designed to meet all requirements of the Audio Codec ’97, Component Specification, Revision 1.03, © 1996, Intel Cor-poration, found at www.Intel.com. The AD1881 also includes some other Codec enhanced features such as communicating to three Codecs on the same link, a DSP serial port mode, modem sample rates and filtering, and built-in Phat Stereo 3D enhancement.
Suggested Replacement Parts
AC’97 SoundMAX® Codec
Documentation
Obsolete Data Sheet 1
This is the most up-to-date revision of the Data Sheet.
Latest Discussions
No discussions on ad1881 yet. Have something to say?
Start a Discussion on EngineerZone®